Real Time

Power Relevant Parameters (Basic LTE FDD Downlink)

Additional Downlink Setup parameters are described in Cell Parameters (Basic LTE FDD Downlink), Cell Specific Reference Signal (Basic LTE FDD Downlink), and Synchronization Signals (Basic LTE FDD Downlink).

Power Definition Type

Choice: Total Power | RSTP

Default: Total Power

Double-click or use the drop-down menu to select the power definition type.

If Total Power is selected, power reference is Amplitude parameter on Instrument node. In this case, RSTP and OSTP are automatically calculated by Amplitude parameter on Instrument node, Power parameter on Carrier node and each carrier signal settings.

If RSTP is selected, power reference is RSTP. In this case, Amplitude on Instrument node and OSTP are calculated by RSTP, Power parameter on Carrier node and each carrier signal settings.

In multiple carrier case, Power Definition Type parameter in each carrier should be same.

Reference Signal Transmit Power (RSTP)

Range: -15.00 to -144.00 dBm

Default: -34.77 dBm

Enter the Reference Signal Transmit Power in dBm, when the Power Definition Type is RSTP. Otherwise displays the Reference Signal Transmit Power in dBm and the value is updated after generation.

Available setting range and step depends on hardware.

See 3GPP TS 36.141 for more information.

OFDM Symbol Transmit Power (OSTP)

This parameter is set by the software.

PDSCH Cell Specific Ratio

Choice: pB/pA=1 | P_B=0 | P_B=1 | P_B=2 | P_B=3

Default: pB/pA=1

Double-click or use the drop-down menu to select the PDSCH cell specific ratio.